< Assembler Command Options / Object Options >
[Format]
 
If this option is not specified, additional information for the inter-module optimization is not output.
[Description]
-  | This option outputs the additional information for the inter-module optimization.  | 
 
-  | At linkage, inter-module optimization is applied to the file specified with this option.  |