|
|
|
|
|
Source Options
|
-include
|
Specifies the names of folders that hold include files.
|
|
-define
|
Specifies macro definitions.
|
|
-chkpm
|
Checks for a privileged instruction.
|
|
-chkfpu
|
Checks for a floating-point operation instruction.
|
|
-chkdsp
|
Checks for a DSP instruction.
|
|
Object Options
|
-output
|
Specifies the relocatable file name.
|
|
-debug
|
Debugging information is output to the object files.
|
|
-nodebug
|
Debugging information is not output to the object files.
|
|
-goptimize
|
Outputs additional information for inter-module optimization.
|
|
-fpu
|
Generates a relocatable file which is capable of containing FPU instructions.
|
|
-nofpu
|
Generates a relocatable file which is not capable of containing FPU instructions.
|
|
-create_unfilled_area
|
[To be supported by V2.03 and later versions]
Makes spaces created by .OFFSET unfilled.
|
|
List Options
|
-listfile
|
An assembler list file is output.
|
|
-nolistfile
|
An assembler list file is not output.
|
|
-show
|
Specifies the contents of the source list file.
|
|
Microcontroller Options
|
-isa
|
Selects the instruction-set architecture.
|
|
-cpu
|
Selects the microcontroller type.
|
|
-endian
|
Selects the endian type.
|
|
-fint_register
|
Selects a general register for exclusive use with the fast interrupt function.
|
|
-base
|
Specifies the base registers for ROM and RAM.
|
|
-patch
|
Selects avoidance or non-avoidance of a problem specific to the CPU type.
|
|
-pic
|
Enables the PIC function.
|
|
-pid
|
Enables the PID function.
|
|
-nouse_pid_register
|
The PID register is not used in code generation.
|
|
Other Options
|
-logo
|
Selects the output of copyright information.
|
|
-nologo
|
Selects the non-output of copyright information.
|
|
-subcommand
|
Specifies a file for including command options.
|
|
-euc
|
The character codes of input programs are interpreted as EUC codes.
|
|
-sjis
|
The character codes of input programs are interpreted as SJIS codes.
|
|
-latin1
|
The character codes of input programs are interpreted as ISO-Latin1 codes.
|
|
-big5
|
The character codes of input programs are interpreted as BIG5 codes.
|
|
-gb2312
|
The character codes of input programs are interpreted as GB2312 codes.
|
|
-utf8 [V2.04.00 or later]
|
The character codes of input programs are interpreted as UTF-8 codes.
|