< Assembler Command Options / List Options >
[Format]
-show=<sub>[,...] 
      <sub>: { conditionals | definitions | expansions }
 | 
 
[Description]
-  | This option specifies the contents of the list file to be output by the assembler. The following output types can be specified as <sub>.  | 
 
Table 2.12  | Output Types Specifiable for show Option  | 
 
| 
 | 
 | 
| 
 
conditionals 
 | 
 
The statements for which the specified condition is not satisfied in conditional assembly are also output to a source list file. 
 | 
| 
 
definitions 
 | 
 
The information before replacement specified by .DEFINE is output to a source list file. 
 | 
| 
 
expansions 
 | 
 
The macro expansion statements are output to a source list file. 
 |