< Optimizing Linkage Editor (rlink) Options / Output Options >
The default values are FF (hexadecimal) for Intel HEX-format files and 10 (hexadecimal) for Motorola S-format files.
This option is used to specify the length of data records in Intel HEX-format files or Motorola S-format files to be generated. |
Specifying 16 bytes (10 in hexadecimal) as the length of data records
This option is invalid for file formats other than Intel HEX type (form=hex) or Motorola S-record type (form=stype). |