< Optimizing Linkage Editor (rlink) Options / Output Options >
This option specifies object files to be exempted from the function list for use in detecting illegal indirect function calls. |
For details on detecting illegal indirect function calls, refer to the item on the '-control_flow_integrity [Professional Edition only] [V2.08.00 or later]' compiler option.
If this option is specified more than once, the functions of all specified object files are exempted from the function list. |
When this option is used, the -cfi option must also be specified. If the -cfi option is not specified, an error will occur. |