[Eventflag] tab

This tab displays the eventflag information (e.g. Eventflag Name and ID) of the RI78V4.

Figure A-7. [Eventflag] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

(a) First layer

This layer displays the eventflag information (e.g. Eventflag Name and ID) of the RI78V4.

This layer consists of the following items.

Eventflag Name

An icon indicating the current status of the eventflag and the name of the eventflag are shown in the following format.

Icon Name

Note that if the name of eventflag is undefined, the name will appear as "ID".

There are waiting tasks.

There are no waiting tasks.

ID

The ID of the eventflag is shown.

Queue Status

The current status of the eventflag is shown.

Waiting Tasks

There are waiting tasks.

Empty

There are no waiting tasks.

Current Flag Pattern

The current bit pattern of the eventflag is shown.

Initial Flag Pattern

The initial bit pattern "0x0000" of the eventflag is shown.

Attribute

The attributes of the eventflag (task queuing method, maximum number of tasks that can be queued and bit pattern clearing flag) are shown in the following format.

Queuing method Maximum number Clearing flag

[Task queuing method]

TA_TFIFO

FIFO order

[Maximum number of tasks that can be queued]

TA_WSGL

Only one task

[Bit pattern clearing flag]

TA_CLR

Bit pattern cleared if the request conditions are met.

Nothing displayed

Bit pattern not cleared if the request conditions are met.



(b) Second layer

The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the eventflag's wait queue.

See the [Task] tab for details about waiting task information.

Figure A-8. [Eventflag] Tab (Waiting Task Information)



Remarks 1. If the waiting task information (Task Name, ID, Status, Wait Factor, Wait Data, Time Left, Interrupt, Current Priority, Task Start Address, Current PC) in each cell is double clicked, then Editor panel displays the source file of the task, and the caret moves to the corresponding location.

2. If the waiting task information (Current Task SP) in the cell is double clicked, then Memory panel displays the contents of the task stack, and the caret moves to the corresponding location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Eventflag Name, ID, Queue Status, Current Flag Pattern, Initial Flag Pattern, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

ID, Current Flag Pattern, Initial Flag Pattern

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).