[Initialize Routine] tab

This tab displays the initialize routine information (e.g. Start Address and Extended Information) of the RI78V4.

Figure A-20. [Initialize Routine] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

This area displays the initialize routine information (e.g. Start Address and Extended Information) of the RI78V4.

This area consists of the following items.

Start Address

An icon and the start address of the initialize routine are shown in the following format.

Icon Start address

Extended Information

"-" is shown.

Attribute

"-" is shown.



Remark If the initialize routine information (e.g. Start Address and Extended Information) in each cell is double clicked, then Editor panel displays the source file of the initialize routine, and the caret moves to the corresponding location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Start Address, Extended Information, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

Start Address, Extended Information

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Jump to Source (Start Address)

Opens the Editor panel, and displays the source code of the initialize routine.

Jump to Disassemble (Start Address)

Opens the Disassemble panel, and displays the results of disassembling the initialize routine.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).