Column Number Settings dialog box


This dialog box is used to set the number of view columns of memory values on the Memory panel.

Figure A.34

Column Number Settings Dialog Box

 

This section describes the following.

[How to open]

-

On the Memory panel, select [View] >> [Column Number Settings…] from the context menu.

[Description of each area]

(1)

[Column Number] area

Directly enter a decimal value as the number of columns you want to display.

The settable range depends on [Size Notation] currently being set on the Memory panel, as follows:

Size Notation

Settable Range

4 Bits

2 - 512Note

1 Byte

1 - 256

2 Bytes

1 - 128

4 Bytes

1 - 64

8 Bytes

1 - 32

Note

Only an even number is specifiable (if an odd number is specified, then it will be changed to a value one greater than such odd number).

[Function buttons]

Button

Function

OK

Displays memory values in the specified number of columns.

Cancel

Cancels the settings and closes this dialog box.

Help

Displays the help for this dialog box.