Project Tree panel


This panel is used to display the project components (microcontroller, build tool, debug tool, etc.) in a tree structure.

On this panel, you can select or change the debug tool to use.

Figure A.3

Project Tree Panel

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Project Tree].

[Description of each area]

(1)

Project tree area

Project components are displayed in tree view with the following given node.

Node

Description

RL78 Debug tool name (Debug tool)

Debug tool name:

The debug tool (IECUBE, E2, E2 Lite, E1(Serial), E20(Serial), EZ Emulator or Simulator) currently being used in the project is displayed.
[Simulator] is selected by default.

 

Select the debug tool node to configure with the Property panel. If the Property panel is not being opened, double-click the node to open the corresponding Property panel.

[Context menu]

Using Debug Tool

The following cascade menus are displayed to select the debug tool to use.

 

RL78 IECUBE

Uses IECUBE as the debug tool.

RL78 E2

Uses E2 as the debug tool.

RL78 E2 Lite

Uses E2 Lite as the debug tool.

RL78 E1(Serial)

Uses E1 with serial communication method as the debug tool.

RL78 E20(Serial)

Uses E20 with serial communication method as the debug tool.

RL78 EZ Emulator

Uses EZ Emulator with an evaluation kit and so on.

RL78 Simulator

Uses Simulator as the debug tool.

Property

Displays the selected category node's property in the Property panel.