Loop dialog box


This dialog box is used to perform detailed settings (loop start/stop and loop count) related to the loop information in the Signal Data Editor window.

Figure A.64

Loop Dialog Box

 

This section describes the following.

[How to open]

On the Signal Data Editor window, any one of the following:

-

Double-click the Mark area.

-

Select the Mark area, then select [Mark] >> [Loop Dialog...] from the [Edit] menu.

[Description of each area]

(1)

Loop information setting area

Start of Loop

Select this check box to set the Start of Loop.

Endless loop

Select this option button to set the Endless Loop.

Loop count

Select this option button to set the Loop Count.

Sets the count value by spin button.

0

Skip loop

1 to 99

Perform loop the specified count.

End of Loop

Select this check box to set the End of Loop.

[Function buttons]

Button

Function

OK

Validates the settings and closes this dialog box.

Cancel

Cancels the settings and closes this dialog box.