2.3.5.1 [Connect Settings] tab

In the [Connect Settings] tab, you can configure the connection with the debug tool for each one of the following categories.

 

(1) [Internal ROM/RAM]

(2) [Endian]

(3) [Clock]

(4) [Peripheral Function Simulation]

(1)

[Internal ROM/RAM]

The size of internal ROM/RAM of the selected microcontroller is displayed in this category.

Figure 2.59

[Internal ROM/RAM] Category [Simulator]

(a)

[Size of internal ROM[KBytes]

The internal ROM size to simulate is displayed (unit: Kbytes).

You cannot change the value of this property.

(b)

[Size of internal RAM[KBytes]]

The internal RAM size to simulate is displayed (unit: Kbytes).

You cannot change the value of this property.

(2)

[Endian]

You can configure endian in this category.

Figure 2.60

[Endian] Category [Simulator]

(a)

[Endian of CPU]

Specify the endian for the CPU.

By default, the endian selected in the build tool property is displayed.

Caution

You cannot change this property while connected to the Simulator.

(3)

[Clock]

You can configure clock in this category.

Figure 2.61

[Clock] Category [Simulator]

(a)

[System clock (ICLK) frequency [MHz]]

Specify the clock frequency for the CPU (unit: MHz).

You can specify a desired frequency value.

Enter an integer directly in the range 1 to 1,000.

Caution

You cannot change this property while connected to the Simulator.

(4)

[Peripheral Function Simulation]

You can configure simulation of peripheral functions in this category.

Figure 2.62

[Peripheral Function Simulation] Category

(a)

[Peripheral function simulation module]

It displays the name of available peripheral function simulation modules and lets you select from the drop-down list whether to use each module being displayed.

Select [Use] when using the module ([Not Use] is selected by default).

You cannot change the name of peripheral function simulation modules on this panel.

(b)

[Peripheral clock rate]

Specify from the drop-down list the peripheral-to-internal clock ratio that shows the number of internal clock that is equivalent to 1 peripheral clock.

The following clock rates are displayed in the drop-down list.

1(Default), 2, 3, 4, 6, 8, 12, 16, 24, 32, 64

Caution

You cannot change this property while connected to the Simulator.