In the Editor panel/Disassemble panel, set an interrupt event at a location where you want an interrupt request to be generated.
In the Editor panel/Disassemble panel, move the caret to the line/addressNote at which you want to set an interrupt event and then select [Register Action Event...] from the context menu to open the following Action Events dialog box, then select the [Interrupt event setting] tab [Simulator].
In this dialog box, follow the steps below.
Specify the interrupt vector by directly entering a corresponding number between 0 and 255.
Specify an interrupt's priority level.
Specify the priority order by directly entering a number between 1 and 8.
When 8 is specified, the event is handled as a fast interrupt.
Specify the priority order by directly entering a number between 1 and 16.
When 16 is specified, the event is handled as a fast interrupt.
Set the interrupt event to the line at the caret position in the Editor panel/Disassemble panel.
When the interrupt event is set, the
mark is displayed in the event area on the Editor panel/Disassemble panel, and the set interrupt event is managed in the Events panel (see "2.17 Event Management").