Action Events dialog box


You can set action events in this dialog box (see "2.16 Set an Action into Programs").

This dialog box can be opened only when you are connected to the debug tool.

Caution

Also see "2.17.7 Points to note regarding event setting" for details on action event settings, including the allowable number of valid events.

Figure A.46

Action Events Dialog Box

 

This section describes the following.

[How to open]

-

On the Editor panel, move the caret to the line where you wish to set an action event, then select [Register Action Event...] from the context menu.

-

On the Disassemble panel, move the caret to the address where you wish to set a Printf event, then select [Register Action Event...] from the context menu.

-

On the Events panel, select [Edit Condition...] from the context menu after selecting the action event.

[Description of each area]

(1)

Tab selection area

You can switch action events to be registered by the selection of a tab. This dialog box has the following tabs.

Caution

When you open this dialog box by selecting [Edit Condition...] from the context menu, this area will be hidden.

(2)

[Event conditions settings] area

You can set detailed conditions for each action event in this area. See the section of the corresponding tab for the details of the setting procedure.

[Function buttons]

Button

Function

OK

Ends the setting of the action event and sets the specified action event at a specified location.

Cancel

Cancels the action event setup and closes this dialog box.

Help

Displays the help for this dialog box.