Renesas Electronics
Below is a list of CS+ Python classes.
Table B.6
CS+ Python Class
Class Name
Function Description
ActionEventCondition
This class creates an action event condition.
ActionEventInfo
This class holds action event information.
ActionInfo
This class holds result information of the action event.
BreakCondition
This class creates a break condition.
BreakpointInfo
This class holds break point information.
BuildCompletedEventArgs
This class holds the parameters when a build completes.
CurrentConsumptionInfo
This class holds information of current consumption data.
DisassembleInfo
This class holds disassembly information.
DownloadCondition
This class creates conditions of the download file.
DownloadInfo
This class holds download information.
FunctionInfo
This class holds function information.
IORInfo
This class holds IOR and SFR information.
MapInfo
This class holds map information.
PerformanceCondition
This class creates conditions of performance measurement.
PerformanceEventInfo
This class holds performance measurement event information.
PerformanceInfo
This class holds performance measurement information.
PseudoErrorCondition
This class creates a pseudo-error condition.
PseudoErrorInfo
This class holds ECM error information.
SoftwareTraceEventInfo
This class holds software trace event information.
SoftwareTraceInfo
This class holds software trace information or software trace (LPD output) information.
SoftwareTraceLPDEventInfo
This class holds software trace (LPD output) event information.
StackInfo
This class holds stack information.
TimerCondition
This class creates conditions of a conditional timer.
TimerEventInfo
This class holds conditional timer event information.
TimerInfo
This class holds conditional timer information.
TraceCondition
This class creates conditions of a conditional trace.
TraceEventInfo
This class holds conditional trace event information.
TraceInfo
This class holds trace information.
VariableInfo
This class holds variable information.
XRunBreakInfo
This class holds XRunBreak information.
XTimeInfo
This class holds timer information.