Editing the Program

In this section, you edit the user program.

First, the basic editing method is explained, and then you edit the program through a simple copy and paste procedure. Edit the program following the steps listed below.

1. How to open a source code file

The following step describes how to open a source code file.

Find the source code file you want to edit in the Project Tree and double-click it.

This displays the source code in the Main panel.