Editing the Program

2. Editing

Edit the program following the steps listed below.

Double-click "r_main.c" in the Project Tree.

Copy the following text and paste it to the section of r_main.c shown in the figure below.

R_TAU0_Channel0_Start();

Double-click "r_timer_user.c" in the Project Tree.

Copy the following texts and paste them to the sections of r_timer_user.c shown in the figure below.

uint16_t g_count;

uint16_t inreg = 0,outreg = 0;

inreg = P6_bit.no2;

outreg = inreg ^ 1;

P6_bit.no2 = outreg;

P6_bit.no3 = inreg;

g_count++;