Renesas Electronics
top
License Manager
FUNCTIONS
Using a License Manager
2.3
Using a License Manager
This section describes how to use a license manager.
Differences Information
Previous Topic
Uninstalling License Manager
Next Topic
Confirming the status
Table of Contents
Installing License Manager
Uninstalling License Manager
Using a License Manager
Confirming the status
Showing information on the expiration of annual licenses
Add a node locked license
Delete a node locked license
Setting up the floating license
Acquiring a floating license
Acquiring a floating license for use in offline mode
Ending use of a floating license in offline mode
Indicating mismatches between versions registered with the license manager and the floating license server
Change options
Resetting When the Server Is Changed