2.6 Customize Display Method

The following operations will enable you to customize the displaying of items (columns) and the analysis information on the Function List panel/Variable List panel.

All operations refer to the header area of each panel (the area where the column labels are displayed).

Remark

In the Column Chooser dialog box, click the [Default] button to return all the customizations you have performed via the operations above to the default values.