Input on the command line should be made as follows.
... : Pattern in proceeding [ ] can be repeated
{ } : Select from items delimited by the pipe symbol ("|")
| Any file names supported by Windows are allowed as input file names or file names to be specified for options. | 
| Input file names and file names to be specified for options can also be specified with an absolute path or relative path. When specifying an input file name or a file name to be specified for an option without the path or with a relative path, the reference point of the path is the current folder. | 
| When a space is included in an input file name or a file name to be specified for an option (including the path name), enclose the file name including the path name in a pair of double quotation marks ("). | 
| The maximum length of an input file name or a file name to be specified for an option depends on Windows (up to 259 characters). | 
| An error will occur when more than one input file name is specified. Use the -l option to specify multiple input file names. | 
| When an input file is specified, it is certainly necessary to specify an output file name. When an input file has been specified on the command line, use the -o option to specify the output file. |