This section explains CcnvCA78K0 options.
 
| 
- | Uppercase characters and lowercase characters are distinguished for options. | 
| 
- | When a file name is specified as a parameter, it can include the path (absolute path or relative path). When a file name without the path or a relative path is specified, the reference point of the path is the current folder.  | 
| 
- | When a parameter includes a space (such as a path name), enclose the parameter in a pair of double quotation marks ("). | 
 
|  |  | 
| 
-V | 
This option displays the version information of CcnvCA78K0. | 
| 
-h | 
This option displays the descriptions of CcnvCA78K0 options. | 
| 
-c | 
This option specifies the Japanese character code. | 
| 
-l | 
This option specifies the list file name. | 
| 
-o | 
This option specifies the output file name. | 
| 
-r | 
This option specifies where the message is to be output. | 
| 
-A | 
This option performs conversion with the functions related to the ANSI standard enabled. |