This option performs conversion with the -za option (which is an ANSI-compliant option of CA78K0) enabled.
Conversion is performed with the -za option disabled.
| When this option is specified, the following words are not regarded as keywords and they will not be converted. | 
| Specify this option if the -za option is used in the CA78K0 development environment before conversion. |