-o


This option specifies the output file name.

[Specification format]

-o=file

 

-

Interpretation when omitted

This option cannot be omitted except for when the -V, -h, or -l option is specified. An error will occur if this option is omitted.

[Detailed description]

-

This option specifies the output file name after conversion.

-

If the specified file already exists, it will be overwritten and no warning is output.

-

An error will occur if the output file name matches the input file name or the file name specified by the -r option.

-

When this option is specified simultaneously with the -l option, a warning is output and this -o option is ignored.

-

An error will occur if the parameter is omitted.

[Example of use]

>CcnvCA78K0R  input.c  -o=output.c