r_cgc_ram_ecc_interrupt

Performs processing in response to the RAM 1-bit correction/2-bit error detection interrupt INTRAM.

Remark This API function is called as the interrupt process corresponding to the RAM 1-bit correction/2-bit error detection interrupt INTRAM.

[Syntax]

CA78K0R Compiler

__interrupt static void r_cgc_ram_ecc_interrupt ( void );

CC-RL Compiler

static void __near r_cgc_ram_ecc_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.