Below is a list of API functions output by the Code Generator for clock generator (include reset function, on-chip debug function, etc.) use.
Table 3.2 API Functions: [Clock Generator]
|
API Function Name |
Function |
|
Performs initialization required to control the clock generator (include reset function, on-chip debug function, etc.). | |
|
Performs user-defined initialization relating to the clock generator (include reset function, on-chip debug function, etc.). | |
|
Performs processing in response to the RAM 1-bit correction/2-bit error detection interrupt INTRAM. | |
|
Performs processing in response to the stackpointer overflow/underflow interrupt INTSPM. | |
|
Performs processing in response to the clock monitor interrupt INTCLM. | |
|
Performs processing in response to RESET signal. | |
|
Changes the CPU clock/peripheral hardware clock. | |
|
Starts the RAM-ECC function. | |
|
Ends the RAM-ECC function. | |
|
Starts the CPU stack pointer monitor function. | |
|
Ends the CPU stack pointer monitor function. | |
|
Starts the clock monitor. | |
|
Ends the clock monitor. |