Sets the analog voltage output to the ANOn pin.
[Syntax]
#include r_cg_macrodriver.h
void R_DACn_Set_ConversionValue ( uint8_t reg_value );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
I |
Uint8_t reg_value; |
D/A conversion value (0x0 to 0xFF) |
[Return value]
None.