Usage example

Start conversion digital input to analog signal from 0x00. Add 0x10 to digital input at fixed interval. Stop conversion when digital input becomes 0xFF.

[GUI setting example]

D/A convertor

Used

DAC

Used

DAC0

D/A convertor operation setting

Used

D/A convertor operation setting

Normal mode

Analog output (ANO0)

Used

Conversion value

0x00

Timer

Used

TAU0

Used

Channel0

channel 0

Interval timer

Interval value (16 bits)

100ms (Actual value:100)

Generates INTTM00 when counting is started

Unused

End of timer channel 0 count, generate an interrupt (INTTM00)

Used

Priority (INTTM00)

Low

[API setting example]

r_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start TAU0 channel 0 counter */

R_TAU0_Channel0_Start();

/* Enable the DA converter channel 0 */

R_DAC0_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}

r_cg_timer_user.c

/* Start user code for include. Do not edit comment generated here */

#include "r_cg_dac.h"

/* End user code. Do not edit comment generated here */

/* Start user code for global. Do not edit comment generated here */

volatile uint16_t g_dac0_value = _00_DA0_CONVERSION_VALUE;

/* End user code. Do not edit comment generated here */

static void __near r_tau0_channel0_interrupt(void)

{

/* Start user code. Do not edit comment generated here */

g_dac0_value += 0x0010U;

if (g_dac0_value <= 0x00FFU)

{

/* Set the DA converter channel 0 value */

R_DAC0_Set_ConversionValue((uint8_t)g_dac0_value);

}

else

{

/* Stop the DA converter channel 0 */

R_DAC0_Stop();

/* Stop TAU0 channel 0 counter */

R_TAU0_Channel0_Stop();

}

/* End user code. Do not edit comment generated here */

}