r_dalin_callback_receiveend

Performs processing in response to the DALI reception end interrupt INTSRDLn.

Remark This API function is called as the callback routine of interrupt process r_dalin_interrupt_receive corresponding to the DALI reception end interrupt INTSRDLn (performed when number of received data specified by R_DALIn_Receive argument rx_num has been completed).

[Syntax]

static void r_dalin_callback_receiveend ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.