r_dalin_callback_sendend

Performs processing in response to the DALI transmission end interrupt INTSTDLn.

Remark This API function is called as the callback routine of interrupt process r_dalin_interrupt_send corresponding to the DALI transmission end interrupt INTSTDLn (performed when number of transmission data specified by R_DALIn_Send rgument tx_num has been completed).

[Syntax]

static void r_dalin_callback_sendend ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.