r_exsd_interrupt

Performs processing in response to the External signal sampler edge detection interrupt INTEXSD.

Remark This API function is called as the interrupt process corresponding to the External signal sampler edge detection interrupt INTEXSD.

[Syntax]

CA78K0R Compiler

__interrupt static void r_exsd_interrupt ( void );

CC-RL Compiler

static void __near r_exsd_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.