External signal sampler

Below is a list of API functions output by the Code Generator for External signal sampler use.

Table 3.54 API Functions: [External signal sampler]

API Function Name

FUnction

R_EXSD_Create

Performs initialization necessary to control the External signal sampler.

R_EXSD_Create_UserInit

Performs user-defined initialization relating to the External signal sampler.

r_exsd_interrupt

Performs processing in response to the External signal sampler edge detection interrupt INTEXSD.

R_EXSD_Start

Starts External signal sampling.

R_EXSD_Stop

Ends External signal sampling.

R_EXSD_Set_PowerOff

Halts the clock supplied to the External signal sampler.