Renesas Electronics
Performs user-defined initialization relating to the 12-bit interval timer.
Remark This API function is called as the R_IT_Create callback routine.
[Syntax]
void R_IT_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]