Usage example

Use timer as One-shot timer.

[GUI setting example]

12 bit interval timer

Used

IT

Used

Interval timer operation setting

Used

Interval value

100ms (Actual value:100)

Detection of interval signal (INTIT)

Used

Priority

Low

[API setting example]

r_cg_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start IT module operation */

R_IT_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}

r_cg_it_user.c

static void __near r_it_interrupt(void)

{

/* Start user code. Do not edit comment generated here */

/* Stop IT module operation */

R_IT_Stop();

/* End user code. Do not edit comment generated here */

}