R_LCD_Set_PowerOff

Halts the clock supplied to the LCD controller/driver.

Remark 1. Calling this API function changes the LCD controller/driver to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

Remark 2. This API function stops the clock supply to the LCD controller/driver, by operating the RTCEN bit of peripheral enable register n.
For this reason, this API function also stops the clock supply to other peripheral devices sharing the RTCEN bit (e.g. real-time clock).

[Syntax]

void R_LCD_Set_PowerOff ( void );

[Argument(s)]

None.

[Return value]

None.