LCD controller/driver

Below is a list of API functions output by the Code Generator for LCD controller/driver use.

Table 3.35 API Functions: [LCD Controller/Driver]

API Function Name

Function

R_LCD_Create

Performs initialization necessary to control the LCD controller/driver.

R_LCD_Create_UserInit

Performs user-defined initialization relating to the LCD controller/driver.

r_lcd_interrupt

Performs processing in response to the LCD frame interrupt INTLCD.

R_LCD_Start

Sets the LCD controller/driver to display on status.

R_LCD_Stop

Sets the LCD controller/driver to display off status.

R_LCD_Set_VoltageOn

Enables operation of internal voltage boost circuit and capacitor split circuit.

R_LCD_Set_VoltageOff

Disables operation of internal voltage boost circuit and capacitor split circuit.

R_LCD_Set_PowerOff

Halts the clock supplied to the LCD controller/driver.

R_LCD_VoltageOn

Enables operation of internal voltage boost circuit and capacitor split circuit.

R_LCD_VoltageOff

Disables operation of internal voltage boost circuit and capacitor split circuit.