r_lvd_vbatinterrupt

Performs processing in response to the voltage detection of VBAT pin interrupt INTLVDVBAT.

Remark This API function is called as the interrupt process corresponding to the voltage detection of VBAT pin interrupt INTLVDVBAT.

[Syntax]

CA78K0R Compiler

__interrupt static void r_lvd_vbatinterrupt ( void );

CC-RL Compiler

static void __near r_lvd_vbatinterrupt ( void );

[Argument(s)]

None.

[Return value]

None.