r_lvd_vrtcinterrupt

Performs processing in response to the voltage detection of VRTC pin interrupt INTLVDVRTC.

Remark This API function is called as the interrupt process corresponding to the voltage detection of VRTC pin interrupt INTLVDVRTC.

[Syntax]

CA78K0R Compiler

__interrupt static void r_lvd_vrtcinterrupt ( void );

CC-RL Compiler

static void __near r_lvd_vrtcinterrupt ( void );

[Argument(s)]

None.

[Return value]

None.