r_osdc_interrupt

Performs processing in response to the oscillation stop detection interrupt INTOSDC.

Remark This API function is called as the interrupt process corresponding to the oscillation stop detection interrupt INTOSDC.

[Syntax]

CA78K0R Compiler

__interrupt static void r_osdc_interrupt ( void );

CC-RL Compiler

static void __near r_osdc_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.