Oscillation stop detector

Below is a list of API functions output by the Code Generator for oscillation stop detector use.

Table 3.44 API Functions: [Oscillation Stop Detector]

API Function Name

Function

R_OSDC_Create

Performs initialization necessary to control the oscillation stop detector.

R_OSDC_Create_UserInit

Performs user-defined initialization relating to the oscillation stop detector.

r_osdc_interrupt

Performs processing in response to the oscillation stop detection interrupt INTOSDC.

R_OSDC_Start

Enables operation of oscillation stop detector.

R_OSDC_Stop

Disables operation of oscillation stop detector.

R_OSDC_Set_PowerOff

Halts the clock supplied to the oscillation stop detector.

R_OSDC_Reset

Reset the oscillation stop detector.