r_pga_dsad_interrupt_scan

Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.

Remark This API function is called as the interrupt process corresponding to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.

[Syntax]

CA78K0R Compiler

__interrupt static void r_pga_dsad_interrupt_scan ( void );

CC-RL Compiler

static void __near r_pga_dsad_interrupt_scan ( void );

[Argument(s)]

None.

[Return value]

None.