Below is a list of API functions output by the Code Generator for 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier use.
Table 3.21 API Functions: [24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier]
API Function Name |
Function |
Performs initialization necessary to control the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier. | |
Performs user-defined initialization relating to the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier. | |
Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD. | |
Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS. | |
Starts A/D conversion. | |
Ends A/D conversion. | |
Halts the clock supplied to the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier. | |
Reads the results of A/D conversion.(mean value) | |
Reads the results of A/D conversion. | |
Connects the configurable amplifier to the 24-bit ΔΣ A/D converter and trims the offset. | |
Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD. | |
Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS. |