R_SPI_Create_UserInit

Performs user-defined initialization relating to the SPI interface.

Remark This API function is called as the R_SPI_Create callback routine.

[Syntax]

void R_SPI_Create_UserInit ( void );

[Argument(s)]

None.

[Return value]

None.