Usage example

Transfer and write data ot external device by SPI transmission. After that, read the data for verify check.

※Please use SA-Designer together.

[GUI setting example]

SPI interface

SPI

Used

Analog IC operation setting

Used

Baudrate

300(bps) (Actual value:300.481)

[API setting example]

r_cg_main.c

/* Start user code for global. Do not edit comment generated here */

uint8_t g_flag;

smartanalog_t gp_sa_read_buf[];

extern const smartanalog_t gp_smartanalog_data[];

/* End user code. Do not edit comment generated here */

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

while (1U)

{

if (1U == g_flag)

{

/* Write SAIC register */

R_SAIC_Write(gp_smartanalog_data);

/* Read SAIC register */

R_SAIC_Read(gp_smartanalog_data, gp_sa_read_buf);

/** read after write verify **/

}

}

/* End user code. Do not edit comment generated here */

}