Renesas Electronics
Performs user-defined initialization relating to the 16-bit timer KC0.
Remark This API function is called as the R_TMR_KC0_Create callback routine.
[Syntax]
void R_TMR_KC0_Create_UserInit ( void );
[Argument(s)]
None.
[Return value]