R_TMR_KC0_Set_PowerOff

Halts the clock supplied to the 16-bit timer KC0.

Remark Calling this API function changes the 16-bit timer KC0 to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void R_TMR_KC0_Set_PowerOff ( void );

[Argument(s)]

None.

[Return value]

None.