r_tmr_rjn_interrupt

Performs processing in response to the timer interrupt.

Remark This API function is called as the interrupt process corresponding to the timer interrupt.

[Syntax]

CA78K0R Compiler

__interrupt static void r_tmr_rjn_interrupt ( void );

CC-RL Compiler

static void __near r_tmr_rjn_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.