Below is a list of API functions output by the Code Generator for timer RJ use.
Table 3.6 API Functions: [Timer RJ]
API Function Name |
Function |
Performs initialization necessary to control the 16-bit timer RJn. | |
Performs user-defined initialization relating to the 16-bit timer RJn. | |
Performs processing in response to the timer interrupt. | |
Starts the count for 16-bit timer RJn. | |
Ends the count for 16-bit timer RJn. | |
Halts the clock supplied to the 16-bit timer RJn. | |
Reads the pulse width of the 16-bit timer RJn. | |
Performs initialization necessary to control the 16-bit timer RJn. | |
Performs user-defined initialization relating to the 16-bit timer RJn. | |
Performs processing in response to the timer interrupt. | |
Starts the count for 16-bit timer RJn. | |
Ends the count for 16-bit timer RJn. | |
Halts the clock supplied to the 16-bit timer RJn. | |
Reads the pulse width of the 16-bit timer RJn. |