Below is a list of API functions output by the Code Generator for general PWM timer use.
Table 3.16 API Functions: [General PWM timer]
|
API Function Name |
Function |
|
Performs initialization necessary to control the general PWM timer. | |
|
Starts counting by a 16-bit timer. | |
|
Ends counting by a 16-bit timer. | |
|
Allows GPT interrupts. | |
|
Prohibits GPT interrupts. | |
|
Performs user-defined initialization relating to the general PWM timer. | |
|
Performs processing in response to the input capture/compare match interrupt. | |
|
Performs processing in response to the overflow interrupt. | |
|
Performs processing in response to the underflow interrupt. | |
|
Performs processing in response to the dead time error interrupt. | |
|
Performs processing in response to the external trigger rising interrupt. | |
|
Performs processing in response to the external trigger falling interrupt. |