Below is a list of API functions output by the Code Generator for realtime clock use.
Table 3.22 API Functions: [Realtime Clock]
|
API Function Name |
Function |
|
Performs initialization necessary to control the realtime clock. | |
|
Performs user-defined initialization relating to the realtime clock. | |
|
Performs processing in response to the alarm interrupt (ALM). | |
|
Performs processing in response to the periodic interrupt (PRD). | |
|
Performs processing in response to the carry interrupt (CUP). | |
|
Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (calendar count mode). | |
|
Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (binary count mode). | |
|
Sets the period of the periodic interrupt (PRD) and allows detection of PRD. | |
|
Prohibits detection of the periodic interrupt (PRD). | |
|
Allows detection of the carry interrupt (CUP). | |
|
Prohibits detection of the carry interrupt (CUP). | |
|
Set the RTCOUT output period and starts RTCOUT output. | |
|
Ends the RTCOUT output. | |
|
Starts counting. | |
|
Ends counting. | |
|
Initializes the counter then starts counting. | |
|
Sets the values of the calendar and time counters. | |
|
Gets the values of the calendar and time counters. | |
|
Sets the value of the binary counter. | |
|
Gets the value of the binary counter. | |
|
Gets the captured calendar time value. | |
|
Gets the captured binary time value. |