Option strings specified by a command line or subcommand file are output.
The output example of the option information when they are specified by a command line or subcommand file as follows is shown below.
 
<Command line>
| >rlink -subcommand=test.sub -list -show | 
 
<Subcommand file "test.sub">
| form library input extmod1 input extmod2 output usrlib.lib | 
 
| *** Options ***   -subcommand=test.sub    (1) form library            (2) input extmod1           (2) input extmod2           (2) output usrlib.lib       (2) -list                   (1) -show                   (1) | 
|  |  | 
|  | 
Options specified by command line 
The options specified by the command line are output (in their specified order). | 
|  | 
Options specified in subcommand file 
The options specified in subcommand file "test.sub" are output. |