3.4.4  
Library information
 
The type of the library is output.
The output example of the library information is shown below.
| *** Library Information ***   LIBRARY NAME=usrlib.lib (1) CPU=RH850               (2) ENDIAN=Little           (3) ATTRIBUTE=user          (4) NUMBER OF MODULE=2      (5) | 
|  |  | 
|  | 
Library name 
The library name is output. | 
|  | 
Microcontroller name 
The microcontroller name is output. | 
|  | 
Endian type 
The endian type is output. | 
|  | 
Library file attribute 
Either a system library or user library is output. | 
|  | 
Number of modules within library 
The number of modules within the library is output. |